I'm trying to run the GenCodecPkg wizard from CCSv4 under WindowsXP SP2 per http://processors.wiki.ti.com/index.php/Codec_Engine_GenCodecPkg_Wizard_FAQ#From_CCSv4 .
I downloaded Codec Engine 2.26.02.11. I've set "Tool Discovery Path" (Window | Preferences | CCS | RTSC | Products) to "c:\Program Files\Texas Instruments\codec_engine_2_26_02_11". The "Discovered Tools" list now includes an entry for "Codec Engine". I now have a new "Tools | Codec Engine Tools | GenCodecPkg" menu item. However, when I click on that menu option, nothing happens.
Note I am trying this after freshly loading CCS, with no project open. Please help me get started here.
Please note I've found http://processors.wiki.ti.com/index.php/Getting_started_with_IUNIVERSAL#Step_4:_Customizing_the_Code_to_Fit_Your_Algorithm as well. But the first step is to launch the wizard, and I can't seem to do that.
Please note that my interest is in creating a customized video analytics codec. For example, pass through video and replace red with green. A US flag would look green, white, and blue. I figure I can follow the iUniversal instructions, but work from the ividanalytics_copy example instead.
About ividanalytics_copy, I seem to have at least three copies. Some copies include a CCSv3 project, which I've successfully imported into CCSv4. But these don't have IVIDANALYTICS_COPY.xs or .xdc. Others that do have these files, don't have the example project. Also, I find one with the codec engine I just downloaded, in the folder tree under "sdo" and another under "xdais". Why so many copies of the example? With is right? Is ANY ONE of them complete!!!???!!! Arrgghh! Speaking of "SDO", they tend to blow things up. That's how I'm feeling right now about this! (ref Caprica)
Thanks,
Helmut