Part Number: AM3352
Hi.
Due to we need to modify the UBOOT/SPL menuconfig for SDK6.1.0.8, may you tell us how to modify the menu config the SDK6?
If we use those 3 below command sets, let's say A/B/C, the u-boot/SPL will use the default menuconfig.
A.
make -C /opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/board-support/u-boot-2019.01+gitAUTOINC+029e4c009a-g029e4c009a/ ARCH=arm CROSS_COMPILE=/opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf- menuconfig
B.
make ARCH=arm CROSS_COMPILE=/opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf- mrproper
C..
make -C /opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/board-support/u-boot-2019.01+gitAUTOINC+029e4c009a-g029e4c009a/ ARCH=arm CROSS_COMPILE=/opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-linux-gnueabihf- O=am43xx_evm am43xx_evm_defconfig all
if we use this sequence to modify the menu config: B --> A --> C, the uboot will have the build error, please help us to fix it.
scripts/kconfig/conf --syncconfig Kconfig
CHK include/config.h
CFG u-boot.cfg
GEN include/autoconf.mk
GEN include/autoconf.mk.dep
CFG spl/u-boot.cfg
GEN spl/include/autoconf.mk
CHK include/config/uboot.release
Using .. as source for U-Boot
.. is not clean, please run 'make mrproper'
in the '..' directory.
../Makefile:1563: recipe for target 'prepare3' failed
make[2]: *** [prepare3] Error 1
/opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/board-support/u-boot-2019.01+gitAUTOINC+029e4c009a-g029e4c009a/Makefile:481: recipe for target '__build_one_by_one' failed
make[1]: *** [__build_one_by_one] Error 2
make[1]: Leaving directory '/opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/board-support/u-boot-2019.01+gitAUTOINC+029e4c009a-g029e4c009a/am43xx_evm'
Makefile:148: recipe for target 'sub-make' failed
make: *** [sub-make] Error 2
make: Leaving directory '/opt/ti-processor-sdk-linux-am437x-evm-06.01.00.08/board-support/u-boot-2019.01+gitAUTOINC+029e4c009a-g029e4c009a'
BR Rio