Good Day all
II have seen a post before regarding this question but for the life of me I can't seem to get it again through the search engine.
I am currently using a custom board where we can control the hardware build to add 2G or 4G or Ram at production.
My question
For U-Boot and Kernel release. can one set to detect Populated RAM size and then adjust U-Boot and Kernel parameters for the allocated RAM on board?.
U-Boot : 2018-01
SDK: 5.02.00.10
Regards