Hello,
I want to integrate the current 2.6.36 Linux Kernel with the older DaVinci TI_AM1808_SDK/DaVinci-PSP-SDK-03.20.00.12 of May 2010. While looking at the source, there are some things in the current 2.6.36 Kernel, like drivers/net/davinci.c interrupt coalescing, and other are in the DaVinci branch (2.6.32).
Can someone shed some light into the roadmap for the L138/AM1808 kernel sources? Will the USB2.0 / SPI / McBSP things be merged into the mainstream kernel, or at least into the davinci branch on kernel.org?
Thanks,
heibox