I recently built the Stellaris M3 Simulator-based DSP BIOS 6.x example described on the CCSv4 Developers Site. I would like to develop similar applications on the Cortex A8 ARM core in the OMAP3530. However, when I attempted to create a new project, the RTSC Wizard didn't provide an RTSC Target for the Generic Cortex A8 . Can anyone tell me if DSP BIOS 6.x projects can be supported on the A8?
Thanks