Part Number: TDA4VM
Hi, Sir,
I would like to understand how to test MCU only boot mode in TDA4 EVM.
These are my test procedures
1.Set Boot mode switch as OSPI Flash and MCU only=0(SW8=00000000, SW9=01000000)
The result of booting form MCU to Main domain is successed.
2.Set Boot mode switch as OSPI Flash and MCU only=1(SW8=00000000, SW9=01001000)
The result of booting form MCU to Main domain is failed.
There are not any uart log form MCU Spl.
My questions are
1.Is supported MCU only mode = 1 in PSDK 6.1.1 ?
2. Any application note document for MCU only mode = 1 ?
3. How can I run MCU only mode = 1 correctly on TDA4 EVM ?
Br,
KS.