Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3359, AM3352, TPS65910
We are working with SITARA AM3359 processor.
SDK we are using is ti-processor-sdk-linux-am335x-evm-05.00.00.15. In our board, mmc0 is connected to SD Card and mmc1 is connected to eMMC.
We have booted our customized board through SD Card (i.e. mmc0). But we could not detect mmc1 and got mmc1: error -110 whilst initialising MMC card error. Please find the boot log below and help us to proceed further.
U-Boot SPL 2018.01-00228-g4579b130f0-dirty (May 02 2019 - 11:49:36)
Trying to boot from MMC1
*** Warning - bad CRC, using default environment
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
bootlist count 9,5
U-Boot 2018.01-00228-g4579b130f0-dirty (May 02 2019 - 11:49:36 +0530)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
*** Warning - bad CRC, using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: cpsw, usb_ether
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
** Unable to read file boot.scr **
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3850752 bytes read in 352 ms (10.4 MiB/s)
37553 bytes read in 19 ms (1.9 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8df01000, end 8df0d2b0 ...
Starting kernel ...
[ 0.000000] I can't wait to receive it. Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.40-g4796173fc5 (sbr@sbr-Lenovo-B50-80) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #5 PREEMPT Tue Jun 4 159
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM335x EVM-SK
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x8a800000
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 64960
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=00015aa8-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 197276K/262144K available (8192K kernel code, 318K rwdata, 2436K rodata, 1024K init, 275K bss, 15716K reserved, 49152K cma-rese)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff800000 ( 752 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0900000 (9184 kB)
[ 0.000000] .init : 0xc0c00000 - 0xc0d00000 (1024 kB)
[ 0.000000] .data : 0xc0d00000 - 0xc0d4fb88 ( 319 kB)
[ 0.000000] .bss : 0xc0d4fb88 - 0xc0d9493c ( 276 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000016] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000041] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000055] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000278] timer_probe: no matching timers found
[ 0.000534] Console: colour dummy device 80x30
[ 0.000565] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000576] This ensures that you still see kernel messages. Please
[ 0.000584] update your kernel commandline.
[ 0.000619] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032)
[ 0.118768] pid_max: default: 32768 minimum: 301
[ 0.119009] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.119029] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.119966] CPU: Testing write buffer coherency: ok
[ 0.120783] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.120968] Hierarchical SRCU implementation.
[ 0.121388] EFI services will not be available.
[ 0.123148] devtmpfs: initialized
[ 0.133924] random: get_random_u32 called from bucket_table_alloc+0x8c/0x1ac with crng_init=0
[ 0.134453] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.134808] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.134837] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.139254] pinctrl core: initialized pinctrl subsystem
[ 0.140095] DMI not present or invalid.
[ 0.140582] NET: Registered protocol family 16
[ 0.143343] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.161468] omap_hwmod: debugss: _wait_target_disable failed
[ 0.216015] cpuidle: using governor ladder
[ 0.216061] cpuidle: using governor menu
[ 0.221686] OMAP GPIO hardware version 0.1
[ 0.232950] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_gpmc_pins, deferring probe
[ 0.235749] No ATAGs?
[ 0.235766] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.253232] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.257837] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.258020] media: Linux media interface: v0.10
[ 0.258074] Linux video capture interface: v2.00
[ 0.258215] pps_core: LinuxPPS API ver. 1 registered
[ 0.258227] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.258259] PTP clock support registered
[ 0.258304] EDAC MC: Ver: 3.0.0
[ 0.259016] dmi: Firmware registration failed.
[ 0.259530] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.259948] Advanced Linux Sound Architecture Driver Initialized.
[ 0.261341] clocksource: Switched to clocksource timer1
[ 0.272400] NET: Registered protocol family 2
[ 0.273302] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.273347] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.273384] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.273502] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.273528] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.273711] NET: Registered protocol family 1
[ 0.274205] RPC: Registered named UNIX socket transport module.
[ 0.274224] RPC: Registered udp transport module.
[ 0.274233] RPC: Registered tcp transport module.
[ 0.274242] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.275342] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[ 0.275486] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.277311] workingset: timestamp_bits=14 max_order=16 bucket_order=2
[ 0.283161] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.284061] NFS: Registering the id_resolver key type
[ 0.284111] Key type id_resolver registered
[ 0.284121] Key type id_legacy registered
[ 0.284179] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.286608] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.286631] io scheduler noop registered
[ 0.286643] io scheduler deadline registered
[ 0.286925] io scheduler cfq registered (default)
[ 0.286939] io scheduler mq-deadline registered
[ 0.286950] io scheduler kyber registered
[ 0.288702] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.356921] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.360703] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250
[ 0.992276] console [ttyS0] enabled
[ 0.997034] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 31, base_baud = 3000000) is a 8250
[ 1.007029] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 32, base_baud = 3000000) is a 8250
[ 1.018051] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 1.026672] OF: graph: no port node found in /ocp/lcdc@4830e000
[ 1.032987] OF: graph: no port node found in /ocp/lcdc@4830e000
[ 1.039423] OF: graph: no port node found in /ocp/lcdc@4830e000
[ 1.045446] tilcdc 4830e000.lcdc: no encoders/connectors found
[ 1.063427] brd: module loaded
[ 1.074842] loop: module loaded
[ 1.081146] m25p80 spi0.0: unrecognized JEDEC id bytes(spi-nor.c): ff, ff, ff
[ 1.088678] m25p80: probe of spi0.0 failed with error -2
[ 1.096134] libphy: Fixed MDIO Bus: probed
[ 1.171434] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 1.179141] davinci_mdio 4a101000.mdio: detected phy mask ffffffde
[ 1.187511] libphy: 4a101000.mdio: probed
[ 1.191680] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver TI DP83867
[ 1.199989] davinci_mdio 4a101000.mdio: phy[5]: device 4a101000.mdio:05, driver TI DP83867
[ 1.209399] cpsw 4a100000.ethernet: Detected MACID = 30:45:11:de:3c:49
[ 1.216310] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.222778] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.228081] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.236335] cpsw 4a100000.ethernet: cpsw: Detected MACID = 30:45:11:de:3c:4b
[ 1.245016] i2c /dev entries driver
[ 1.249075] IR NEC protocol handler initialized
[ 1.253707] IR RC5(x/sz) protocol handler initialized
[ 1.258783] IR RC6 protocol handler initialized
[ 1.263354] IR JVC protocol handler initialized
[ 1.267903] IR Sony protocol handler initialized
[ 1.272558] IR SANYO protocol handler initialized
[ 1.277283] IR Sharp protocol handler initialized
[ 1.282025] IR MCE Keyboard/mouse protocol handler initialized
[ 1.287882] IR XMP protocol handler initialized
[ 1.294605] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.301920] sdhci: Secure Digital Host Controller Interface driver
[ 1.308134] sdhci: Copyright(c) Pierre Ossman
[ 1.315041] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.321738] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.331930] NET: Registered protocol family 10
[ 1.338170] Segment Routing with IPv6
[ 1.342114] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.348904] NET: Registered protocol family 17
[ 1.353817] Key type dns_resolver registered
[ 1.358369] omap_voltage_late_init: Voltage driver support not added
[ 1.371547] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.376741] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.411592] tps65910 0-002d: No interrupt support, no core IRQ
[ 1.419803] vrtc: supplied by vbat
[ 1.427150] vio: supplied by vbat
[ 1.432142] vdd1: supplied by vbat
[ 1.437525] vdd2: supplied by vbat
[ 1.444066] random: fast init done
[ 1.447969] vdig1: supplied by vbat
[ 1.453016] vdig2: supplied by vbat
[ 1.458001] vpll: supplied by vbat
[ 1.462931] vdac: supplied by vbat
[ 1.467838] vaux1: supplied by vbat
[ 1.472870] vaux2: supplied by vbat
[ 1.477868] vaux33: supplied by vbat
[ 1.483005] vmmc: supplied by vbat
[ 1.487918] vbb: supplied by vbat
[ 1.493117] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.622743] hctosys: unable to open rtc device (rtc0)
[ 1.628764] lis3_reg: disabling
[ 1.636404] ALSA device list:
[ 1.639466] No soundcards found.
[ 1.644097] Waiting for root device PARTUUID=00015aa8-02...
[ 1.671612] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.684392] mmc0: new high speed SDHC card at address aaaa
[ 1.690553] mmcblk0: mmc0:aaaa SS16G 14.8 GiB
[ 1.699979] mmcblk0: p1 p2
[ 1.762600] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 1.770892] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 1.788480] devtmpfs: mounted
[ 1.793619] Freeing unused kernel memory: 1024K
[ 2.011467] mmc1: error -110 whilst initialising MMC card
[ 2.193096] systemd[1]: System time before build time, advancing clock.
[ 2.265964] systemd[1]: systemd 234 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNU)
[ 2.288008] systemd[1]: Detected architecture arm.
Welcome to Arago 2018.10!
[ 2.332704] systemd[1]: Set hostname to <am335x-evm>.
[ 2.721695] systemd[1]: /lib/systemd/system/gadget-init.service:15: Unknown lvalue 'ExecStopPre' in section 'Service'
[ 3.015539] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.023193] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 3.062443] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.069820] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 3.102072] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.109036] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 3.152202] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 3.182367] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 3.215182] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
Mounting POSIX Message Queue File System...
Mounting Kernel Debug File System...
[ OK ] Created slice User and Session Slice.
[ OK ] Reached target Slices.
[ OK ] Listening on Journal Socket (/dev/log).
[ OK ] Created slice system-getty.slice.
[ OK ] Listening on Journal Socket.
[ OK ] Listening on Process Core Dump Socket.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ OK ] Reached target Swap.
Mounting Temporary Directory (/tmp)...
[ OK ] Listening on udev Control Socket.
Starting Remount Root and Kernel File Systems...
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 3.680018] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Reached target Paths.
Starting Journal Service...
Starting Load Kernel Modules...
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Remount Root and Kernel File Systems.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[ OK ] Started Journal Service.
Starting Apply Kernel Variables...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
Starting Create System Users...
Starting Rebuild Hardware Database...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create System Users.
[ 4.482325] systemd-journald[68]: Received request to flush runtime journal from PID 1
Starting Create Static Device Nodes in /dev...
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
Mounting /media/ram...
Starting udev Kernel Device Manager...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Rebuild Dynamic Linker Cache...
Starting Rebuild Journal Catalog...
Starting Create Volatile Files and Directories...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Rebuild Journal Catalog.
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Rebuild Dynamic Linker Cache.
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Rebuild Hardware Database.
Starting Update is Completed...
Starting udev Coldplug all Devices...
[ OK ] Started Update is Completed.
[ OK ] Found device /dev/ttyS0.
[ OK ] Started udev Coldplug all Devices.
[ OK ] Reached target System Initialization.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Started Daily rotation of log files.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on dropbear.socket.
Starting Network Service...
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Kernel Logging Service.
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
Starting uim-sysfs.service...
[ 11.204974] random: crng init done
[ 11.208422] random: 7 urandom warning(s) missed due to ratelimiting
[ OK ] Started System Logging Service.
Starting RPC Bind Service...
[ OK ] Started D-Bus System Message Bus.
Starting Print notice about GPLv3 packages...
[ OK ] Reached target Containers.
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started Job spooling tools.
[ 13.449714] net eth1: initializing cpsw version 1.12 (0)
Starting Login Service...
[ OK ] Started Network Service.
[ 13.697361] TI DP83867 4a101000.mdio:05: attached PHY driver [TI DP83867] (mii_bus:phy_addr=4a101000.mdio:05, irq=POLL)
[ OK ] Started RPC Bind Service.
[ 14.066210] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ OK ] Found device /dev/ttyS3.
[ 14.386461] net eth0: initializing cpsw version 1.12 (0)
[ 14.526218] TI DP83867 4a101000.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
[ 14.716406] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 15.066335] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ OK ] Found device /dev/mmcblk0p1.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Login Service.
Starting Start USB gadget...
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
Starting Wait for Network to be Configured...
[ OK ] Reached target Network.
Starting Lightning Fast Webserver With Light System Requirements...
[ OK ] Started Redis In-Memory Data Store.
Starting Enable and configure wl18xx bluetooth stack...
Starting Simple Network Management Protocol (SNMP) Daemon....
Starting Permit User Sessions...
Starting Network Name Resolution...
[ OK ] Started Lightning Fast Webserver With Light System Requirements.
[ OK ] Started Permit User Sessions.
[ OK ] Started uim-sysfs.service.
[FAILED] Failed to start Start USB gadget.
See 'systemctl status gadget-init.service' for details.
[ OK ] Started Network Name Resolution.
[ OK ] Started Enable and configure wl18xx bluetooth stack.
[ OK ] Started Simple Network Management Protocol (SNMP) Daemon..
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
bash-dev
bash
binutils
cifs-utils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
findutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gstreamer1.0-libav
gzip
hidapi
libdw1
libelf1
libgdbm-compat4
libgdbm-dev
libgdbm4
libgettextlib
libgettextsrc
libgmp10
libidn11
libmavconn
libmpc3
libmpfr4
libreadline-dev
libreadline7
libunistring2
m4-dev
m4
make
mavlink
mavros-extras
mavros-msgs
mavros
nettle
python3-pycairo
socketcan-interface
which
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Started Print notice about GPLv3 packages.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting rc.pvr.service...
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS0.
[ OK ] Started Serial Getty on ttyS3.
[ OK ] Started rc.pvr.service.
Starting weston.service...
[ OK ] Started weston.service.
Starting telnetd.service...
Starting Matrix GUI...
[ OK ] Started telnetd.service.
Starting busybox-udhcpd.service...
Starting thttpd.service...
[ OK ] Started Matrix GUI.
[ OK ] Started busybox-udhcpd.service.
[ OK ] Started thttpd.service.
Starting rng-tools.service...
[ OK ] Started rng-tools.service.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyS0
Arago 2018.10 am335x-evm ttyS0
am335x-evm login: root
Regards
Vamsi Siddhani