This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6548: ePWM chopping frequency

Part Number: AM6548

Hello TI,

We are working on a custom platform based on the TI's AM6548 reference platform TMDX654GP EVM. The software is based upon the latest release from Texas instruments PROCESSOR-SDK-LINUX-AM65X  06_00_00_07.
We have enabled ehrpwm and generated PWM signals on the desired channels.
We have tried to chop the EPWM frequency by make use of EPWM_PCCTL Register (0x0300003C).
When CHPFREQ field value is 0h(no prescale) the chopped frequency is 15.64 Mhz
if the value is 7h(maximum) the chopped frequency is 1.9 Mhz.
1. Is it possible to generate 300khz signal after chopping or what is the minimum frequency could be generated?
2. Is there any way to divide the system clock frequency(FICLK) which is used to generate carrier clock?
Let me know your thoughts on this.
Regards,
Johni.