This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI Support,
I want to build Yocto Linux for J721E Platform for devices TDA4VM and DRA829V.
I followed the document to build SDK from below link:
http://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Overview_Building_the_SDK.html
However I would like to know the configuration to build for J721E platform.
I have below questions:
1) What is the MACHINE type for this platform? and is MACHINE type same for TDA4VM and DRA829V devices.
2) Which configuration file should I use in below step. and is it same for both devices?
./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-<version>-config.txt
3) Do you have a document for building Yocto Linux for J721E platform?
Thanks and Best Regards
Sami
Hi Sami,
The name of the configuration file is "psdkla-06_01_01_02.txt". You will find it in PSDKLA. I couldn't find it in the "normal" configuration repository (git://arago-project.org/git/projects/oe-layersetup.git)
I used "j7-evm" as MACHINE name for TDA4VM. The linux image, which was built based on this, runs successfully on the TDA4VMEVM.
Greetings
Hi Thomas,
Thanks for your reply.
Yes, psdkla-06_01_01_02.txt is missing in normal configuration repository.
where can I get PSDKLA ?
Best Regards
Sami
Or just use this as psdkla-configuration file: (I had this opened anyway)
# This file takes repo entries in the format # repo name,repo uri,repo branch,repo commit[,layers=layer1:layer2...:layern] bitbake,git://git.openembedded.org/bitbake,1.40,6b045e074c6fea97d4e305a5a3c8bf82135d95eb meta-arago,git://arago-project.org/git/meta-arago.git,thud,ti2019.04,layers=meta-arago-distro:meta-arago-extras meta-psdkla,git://arago-project.org/git/projects/meta-psdkla.git,master,7c0f46dc379402a6b61901e834715945a6f6f748,layers= meta-browser,git://github.com/OSSystems/meta-browser.git,master,26d50665e2f7223c5f4ad7481a8d2431e7cb55fb,layers= meta-qt5,git://github.com/meta-qt5/meta-qt5.git,thud,1520d5b2b2beec5e1c3209d3178219e93ef08bca,layers= meta-virtualization,git://git.yoctoproject.org/meta-virtualization,thud,7685c7d415e0002c448007960837ae8898cd57a5,layers= meta-openembedded,git://git.openembedded.org/meta-openembedded,thud,2d088d252624b19df384aecc434d23afb636178f,layers=meta-networking:meta-python:meta-oe:meta-gnome:meta-filesystems meta-ti,git://git.yoctoproject.org/meta-ti,thud,ti2019.04,layers= meta-linaro,git://git.linaro.org/openembedded/meta-linaro.git,thud,615ea7561b844a3867cee4299d83d605c10b02ab,layers=meta-linaro-toolchain:meta-optee oe-core,git://git.openembedded.org/openembedded-core,thud,f5be8c8309a932cde507ba24d042880a922df0b6,layers=meta OECORELAYERCONF=./sample-files/bblayers.conf.sample OECORELOCALCONF=./sample-files/local-arago64.conf.sample
Greetings