Part Number: TDA3MV
Hi,
I would like to change the issCapture output resolution from 1280*800 to another one, how can I do?
I'm using AR0140 to capture images.
Thank you,
Gary
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA3MV
Hi,
I would like to change the issCapture output resolution from 1280*800 to another one, how can I do?
I'm using AR0140 to capture images.
Thank you,
Gary
Hi Gary,
I think AR0140 is configured for the highest supported resolution. Could you please check if AR0140 supports higher resolution?
Rgds,
Brijesh
Hi Gary,
You could use ISP to resize to smaller resolution.
Or you could crop top-left corner in the capture module.
Rgds,
Brijesh
Hello Gary,
Please refer to AR0140 sensor settings in file ar0140_linear_1280x800_setup.h
The following lines of code can be changed to set sensor output resolution
{0x3004, 0x0020, 0x00}, /* X_ADDR_START */ \
{0x3002, 0x0018, 0x00}, /* Y_ADDR_START */ \
{0x3008, 0x051F, 0x00}, /* X_ADDR_END */ \
{0x3006, 0x0337, 0x00}, /* Y_ADDR_END */ \
Please make sure that sensor resolution is also changed in the functions IssSensor_AR0140_TIDA_Init and IssSensor_AR0140_Init
info->width = 1280;
info->height = 800;
Please also make sure that black line position in the struct aewbConfig_ar0140 is also modified accordingly.
798U, /* Black Line Vertical Start */
This must be equal to (sensor output lines - 2). If you set the sensor output to 640x480, Black Line Vertical Start must be 478.
Regards,
Mayank