This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: Bitbake error

Part Number: PROCESSOR-SDK-AM335X


Hi.

Linux is built according to the following URL.
http://software-dl.ti.com/processor-sdk-linux/esd/docs/04_03_00_05/linux/Overview.html#id13

I'm having trouble getting an error with systemd's do_install.
The build environment is Ubuntu 18.04.
The SDK version is 04.03.00.05.

The error log when system_do_install is executed is as follows.
How can I solve this?

NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: linux-ti-staging-rt-4.9.69+gitAUTOINC+4203cb8c96-r22a.arago1.tisdk22 do_fetch: Failed to fetch URL git://git.ti.com/processor-sdk/processor-sdk-linux.git;protocol=git;branch=processor-sdk-linux-rt-04.03.00, attempting MIRRORS if available
ERROR: systemd-1_230+gitAUTOINC+3a74d4fc90-r0.arago5 do_install: Function failed: do_install (log file is located at /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/temp/log.do_install.2299)
ERROR: Logfile of failure stored in: /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/temp/log.do_install.2299
Log data follows:
| DEBUG: SITE files ['endian-little', 'bit-32', 'arm-common', 'arm-32', 'common-linux', 'common-glibc', 'arm-linux', 'arm-linux-gnueabi', 'common']
| DEBUG: Executing shell function useradd_sysroot
| NOTE: systemd: Performing groupadd with [--root /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/sysroots/am335x-custom -r lock]
| NOTE: systemd: Performing groupadd with [--root /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/sysroots/am335x-custom  -r systemd-journal]
| NOTE: systemd: Performing useradd with [--root /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/sysroots/am335x-custom      --system -d / -M --shell /bin/nologin systemd-network]
| NOTE: systemd: Performing useradd with [--root /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/sysroots/am335x-custom  --system -d / -M --shell /bin/nologin systemd-coredump]
| NOTE: systemd: Performing useradd with [--root /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/sysroots/am335x-custom   --system -d / -M --shell /bin/nologin systemd-network]
| NOTE: systemd: user systemd-network already exists, not re-creating it
| NOTE: systemd: Performing useradd with [--root /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/sysroots/am335x-custom  --system -d / -M --shell /bin/nologin systemd-resolve]
| NOTE: systemd: Performing useradd with [--root /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/sysroots/am335x-custom   --system -d / -M --shell /bin/nologin systemd-bus-proxy]
| Running groupadd commands...
| Running useradd commands...
| DEBUG: Shell function useradd_sysroot finished
| DEBUG: SITE files ['endian-little', 'bit-32', 'arm-common', 'arm-32', 'common-linux', 'common-glibc', 'arm-linux', 'arm-linux-gnueabi', 'common']
| DEBUG: Executing shell function do_install
| NOTE: make -j 12 DESTDIR=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image install
| make --no-print-directory install-recursive
| Making install in .
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin'
|  ./arm-linux-gnueabi-libtool   --mode=install /usr/bin/install -c   libsystemd.la libudev.la '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib'
|  /usr/bin/install -c ../git/src/kernel-install/kernel-install '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c .libs/libsystemd.so.0.15.0 /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/libsystemd.so.0.15.0
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd'
| arm-linux-gnueabi-libtool: install: (cd /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib && { ln -s -f libsystemd.so.0.15.0 libsystemd.so.0 || { rm -f libsystemd.so.0 && ln -s libsystemd.so.0.15.0 libsystemd.so.0; }; })
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/bash-completion/completions'
| arm-linux-gnueabi-libtool: install: (cd /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib && { ln -s -f libsystemd.so.0.15.0 libsystemd.so || { rm -f libsystemd.so && ln -s libsystemd.so.0.15.0 libsystemd.so; }; })
|   ./arm-linux-gnueabi-libtool   --mode=install /usr/bin/install -c systemd systemd-cgroups-agent systemd-initctl systemd-shutdown systemd-remount-fs systemd-reply-password systemd-fsck systemd-ac-power systemd-sysctl systemd-sleep systemd-socket-proxyd systemd-update-done systemd-update-utmp systemd-modules-load systemd-udevd systemd-journald systemd-coredump systemd-vconsole-setup systemd-backlight systemd-hostnamed systemd-networkd systemd-networkd-wait-online systemd-logind systemd-user-sessions '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/systemd/catalog'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/dbus-1/system.d'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/doc/systemd'
|   ./arm-linux-gnueabi-libtool   --mode=install /usr/bin/install -c ata_id cdrom_id collect scsi_id v4l_id mtd_probe '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/dbus-1/system-services'
|  /usr/bin/install -c -m 644 ../git/shell-completion/bash/busctl ../git/shell-completion/bash/journalctl ../git/shell-completion/bash/systemd-analyze ../git/shell-completion/bash/systemd-cat ../git/shell-completion/bash/systemd-cgls ../git/shell-completion/bash/systemd-cgtop ../git/shell-completion/bash/systemd-delta ../git/shell-completion/bash/systemd-detect-virt ../git/shell-completion/bash/systemd-nspawn ../git/shell-completion/bash/systemd-path ../git/shell-completion/bash/systemd-run ../git/shell-completion/bash/udevadm ../git/shell-completion/bash/kernel-install ../git/shell-completion/bash/coredumpctl ../git/shell-completion/bash/hostnamectl ../git/shell-completion/bash/networkctl ../git/shell-completion/bash/loginctl '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/bash-completion/completions'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c .libs/libsystemd.lai /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/libsystemd.la
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/factory/etc'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/factory/etc/pam.d'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/kernel/install.d'
|  /usr/bin/install -c -m 644 ../git/catalog/systemd.bg.catalog ../git/catalog/systemd.be.catalog ../git/catalog/systemd.be@latin.catalog ../git/catalog/systemd.fr.catalog ../git/catalog/systemd.it.catalog ../git/catalog/systemd.pl.catalog ../git/catalog/systemd.pt_BR.catalog ../git/catalog/systemd.ru.catalog ../git/catalog/systemd.zh_CN.catalog ../git/catalog/systemd.zh_TW.catalog ../git/catalog/systemd.catalog '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/systemd/catalog'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c .libs/libudev.so.1.6.4 /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/libudev.so.1.6.4
|  /usr/bin/install -c -m 644 ../git/src/core/org.freedesktop.systemd1.service ../git/src/hostname/org.freedesktop.hostname1.service ../git/src/network/org.freedesktop.network1.service ../git/src/login/org.freedesktop.login1.service '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/dbus-1/system-services'
|  /usr/bin/install -c -m 644 ../git/README ../git/NEWS ../git/CODING_STYLE ../git/LICENSE.LGPL2.1 ../git/LICENSE.GPL2 ../git/DISTRO_PORTING ../git/src/libsystemd/sd-bus/PORTING-DBUS1 ../git/src/libsystemd/sd-bus/DIFFERENCES ../git/src/libsystemd/sd-bus/GVARIANT-SERIALIZATION '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/doc/systemd'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/network'
|  /usr/bin/install -c ../git/src/kernel-install/50-depmod.install ../git/src/kernel-install/90-loaderentry.install '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/kernel/install.d'
|  /usr/bin/install -c -m 644 ../git/factory/etc/pam.d/system-auth ../git/factory/etc/pam.d/other '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/factory/etc/pam.d'
|  /usr/bin/install -c -m 644 ../git/factory/etc/nsswitch.conf '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/factory/etc'
| arm-linux-gnueabi-libtool: install: (cd /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib && { ln -s -f libudev.so.1.6.4 libudev.so.1 || { rm -f libudev.so.1 && ln -s libudev.so.1.6.4 libudev.so.1; }; })
|  /usr/bin/install -c -m 644 ../git/src/core/org.freedesktop.systemd1.conf ../git/src/hostname/org.freedesktop.hostname1.conf ../git/src/network/org.freedesktop.network1.conf ../git/src/login/org.freedesktop.login1.conf '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/dbus-1/system.d'
|  /usr/bin/install -c -m 644 ../git/network/99-default.link ../git/network/80-container-host0.network ../git/network/80-container-ve.network ../git/network/80-container-vz.network '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/network'
| arm-linux-gnueabi-libtool: install: (cd /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib && { ln -s -f libudev.so.1.6.4 libudev.so || { rm -f libudev.so && ln -s libudev.so.1.6.4 libudev.so; }; })
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c .libs/libudev.lai /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/libudev.la
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/pam.d'
|  /usr/bin/install -c -m 644 src/login/systemd-user '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/pam.d'
| arm-linux-gnueabi-libtool: warning: remember to run 'arm-linux-gnueabi-libtool --finish /usr/lib'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c ata_id /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev/ata_id
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/systemd'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-preset'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/sysctl.d'
|  /usr/bin/install -c -m 644 ../git/src/core/system.conf ../git/src/core/user.conf ../git/src/journal/journald.conf ../git/src/coredump/coredump.conf '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/systemd'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c cdrom_id /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev/cdrom_id
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c collect /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev/collect
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-cgroups-agent /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-cgroups-agent
|  /usr/bin/install -c -m 644 ../git/system-preset/90-systemd.preset '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-preset'
|  /usr/bin/install -c -m 644 ../git/sysctl.d/50-default.conf '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/sysctl.d'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c scsi_id /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev/scsi_id
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-initctl /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-initctl
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c v4l_id /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev/v4l_id
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-shutdown /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-shutdown
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/tmpfiles.d'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/udev'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev/hwdb.d'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c mtd_probe /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev/mtd_probe
|  /usr/bin/install -c -m 644 ../git/units/graphical.target ../git/units/multi-user.target ../git/units/emergency.target ../git/units/sysinit.target ../git/units/basic.target ../git/units/getty.target ../git/units/halt.target ../git/units/kexec.target ../git/units/exit.target ../git/units/local-fs.target ../git/units/local-fs-pre.target ../git/units/initrd.target ../git/units/initrd-fs.target ../git/units/initrd-root-device.target ../git/units/initrd-root-fs.target ../git/units/remote-fs.target ../git/units/remote-fs-pre.target ../git/units/network.target ../git/units/network-pre.target ../git/units/network-online.target ../git/units/nss-lookup.target ../git/units/nss-user-lookup.target ../git/units/poweroff.target ../git/units/reboot.target ../git/units/rescue.target ../git/units/rpcbind.target ../git/units/time-sync.target ../git/units/shutdown.target ../git/units/final.target ../git/units/umount.target ../git/units/sigpwr.target ../git/units/sleep.target ../git/units/sockets.target ../git/units/timers.target ../git/units/paths.target ../git/units/suspend.target ../git/units/swap.target ../git/units/slices.target ../git/units/system.slice ../git/units/x-.slice '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system'
|  /usr/bin/install -c -m 644 ../git/tmpfiles.d/systemd-nologin.conf ../git/tmpfiles.d/tmp.conf ../git/tmpfiles.d/x11.conf ../git/tmpfiles.d/var.conf ../git/tmpfiles.d/home.conf ../git/tmpfiles.d/systemd-nspawn.conf ../git/tmpfiles.d/journal-nocow.conf ../git/tmpfiles.d/legacy.conf '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/tmpfiles.d'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-remount-fs /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-remount-fs
|  /usr/bin/install -c -m 644 ../git/src/udev/udev.conf '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/udev'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev/rules.d'
|  /usr/bin/install -c -m 644 ../git/hwdb/20-pci-vendor-model.hwdb ../git/hwdb/20-pci-classes.hwdb ../git/hwdb/20-usb-vendor-model.hwdb ../git/hwdb/20-usb-classes.hwdb ../git/hwdb/20-sdio-vendor-model.hwdb ../git/hwdb/20-sdio-classes.hwdb ../git/hwdb/20-bluetooth-vendor-product.hwdb ../git/hwdb/20-acpi-vendor.hwdb ../git/hwdb/20-OUI.hwdb ../git/hwdb/20-net-ifname.hwdb ../git/hwdb/60-evdev.hwdb ../git/hwdb/60-keyboard.hwdb ../git/hwdb/70-mouse.hwdb ../git/hwdb/70-pointingstick.hwdb '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev/hwdb.d'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/X11/xinit/xinitrc.d'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/systemd/user'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/zsh/site-functions'
|  /usr/bin/install -c -m 644 ../git/rules/50-udev-default.rules ../git/rules/60-block.rules ../git/rules/60-drm.rules ../git/rules/60-evdev.rules ../git/rules/60-persistent-storage-tape.rules ../git/rules/60-persistent-input.rules ../git/rules/60-persistent-alsa.rules ../git/rules/60-persistent-storage.rules ../git/rules/60-serial.rules ../git/rules/64-btrfs.rules ../git/rules/70-mouse.rules ../git/rules/75-net-description.rules ../git/rules/78-sound-card.rules ../git/rules/80-net-setup-link.rules ../git/rules/50-firmware.rules ../git/rules/80-drivers.rules ../git/rules/60-cdrom_id.rules ../git/rules/60-persistent-v4l.rules ../git/rules/75-probe_mtd.rules ../git/src/login/70-uaccess.rules ../git/src/login/70-power-switch.rules '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev/rules.d'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/include'
|  /usr/bin/install -c ../git/xorg/50-systemd-user.sh '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/X11/xinit/xinitrc.d'
|  /usr/bin/install -c -m 644 ../git/units/systemd-initctl.socket ../git/units/syslog.socket ../git/units/dev-hugepages.mount ../git/units/dev-mqueue.mount ../git/units/sys-kernel-config.mount ../git/units/sys-kernel-debug.mount ../git/units/sys-fs-fuse-connections.mount units/tmp.mount ../git/units/var-lib-machines.mount ../git/units/printer.target ../git/units/sound.target ../git/units/bluetooth.target ../git/units/smartcard.target ../git/units/systemd-ask-password-wall.path ../git/units/systemd-ask-password-console.path ../git/units/systemd-udevd-control.socket ../git/units/systemd-udevd-kernel.socket ../git/units/system-update.target ../git/units/initrd-switch-root.target ../git/units/machines.target ../git/units/busnames.target ../git/units/org.freedesktop.hostname1.busname ../git/units/org.freedesktop.systemd1.busname ../git/units/org.freedesktop.network1.busname ../git/units/org.freedesktop.login1.busname ../git/units/ldconfig.service ../git/units/systemd-tmpfiles-clean.timer ../git/units/systemd-journald.socket ../git/units/systemd-journald-dev-log.socket ../git/units/systemd-journald-audit.socket ../git/units/systemd-coredump.socket ../git/units/systemd-networkd.socket ../git/units/user.slice '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system'
|  /usr/bin/install -c -m 644 ../git/units/user/basic.target ../git/units/user/default.target ../git/units/user/exit.target '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/systemd/user'
|  /usr/bin/install -c -m 644 ../git/shell-completion/zsh/_busctl ../git/shell-completion/zsh/_journalctl ../git/shell-completion/zsh/_udevadm ../git/shell-completion/zsh/_kernel-install ../git/shell-completion/zsh/_systemd-nspawn ../git/shell-completion/zsh/_systemd-analyze ../git/shell-completion/zsh/_systemd-run ../git/shell-completion/zsh/_sd_hosts_or_user_at_host ../git/shell-completion/zsh/_sd_outputmodes ../git/shell-completion/zsh/_sd_unit_files ../git/shell-completion/zsh/_systemd-delta ../git/shell-completion/zsh/_systemd ../git/shell-completion/zsh/_systemd-tmpfiles ../git/shell-completion/zsh/_coredumpctl ../git/shell-completion/zsh/_hostnamectl ../git/shell-completion/zsh/_loginctl ../git/shell-completion/zsh/_systemd-inhibit '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/zsh/site-functions'
|  /usr/bin/install -c -m 644 ../git/src/libudev/libudev.h '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/include'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-reply-password /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-reply-password
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-fsck /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-fsck
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/systemd'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/bash-completion/completions'
|  /usr/bin/install -c -m 644 src/login/logind.conf '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/systemd'
|  /usr/bin/install -c -m 644 shell-completion/bash/systemctl '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/bash-completion/completions'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/polkit-1/actions'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-ac-power /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-ac-power
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/rpm/macros.d'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/sysctl.d'
|  /usr/bin/install -c -m 644 src/hostname/org.freedesktop.hostname1.policy src/login/org.freedesktop.login1.policy src/core/org.freedesktop.systemd1.policy '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/polkit-1/actions'
|  /usr/bin/install -c -m 644 src/core/macros.systemd '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/rpm/macros.d'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-sysctl /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-sysctl
|  /usr/bin/install -c -m 644 sysctl.d/50-coredump.conf '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/sysctl.d'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-sleep /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-sleep
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev/rules.d'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/tmpfiles.d'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/security'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/systemd/user'
|  /usr/bin/install -c -m 644 units/getty@.service units/serial-getty@.service units/console-shell.service units/console-getty.service units/container-getty@.service units/systemd-initctl.service units/systemd-remount-fs.service units/systemd-ask-password-wall.service units/systemd-ask-password-console.service units/systemd-sysctl.service units/emergency.service units/rescue.service units/user@.service units/systemd-suspend.service units/systemd-halt.service units/systemd-poweroff.service units/systemd-reboot.service units/systemd-kexec.service units/systemd-exit.service units/systemd-fsck@.service units/systemd-fsck-root.service units/systemd-machine-id-commit.service units/systemd-udevd.service units/systemd-udev-trigger.service units/systemd-udev-settle.service units/systemd-hwdb-update.service units/debug-shell.service units/initrd-parse-etc.service units/initrd-cleanup.service units/initrd-udevadm-cleanup-db.service units/initrd-switch-root.service units/systemd-nspawn@.service units/systemd-update-done.service units/systemd-update-utmp.service units/systemd-update-utmp-runlevel.service units/rc-local.service units/halt-local.service units/systemd-modules-load.service units/kmod-static-nodes.service units/systemd-tmpfiles-setup-dev.service '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/pkgconfig'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-socket-proxyd /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-socket-proxyd
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/zsh/site-functions'
|  /usr/bin/install -c -m 644 rules/99-systemd.rules src/vconsole/90-vconsole.rules src/login/71-seat.rules src/login/73-seat-late.rules '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/udev/rules.d'
|  ./arm-linux-gnueabi-libtool   --mode=install /usr/bin/install -c   pam_systemd.la '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/security'
|  /usr/bin/install -c -m 644 tmpfiles.d/systemd.conf tmpfiles.d/etc.conf '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/tmpfiles.d'
|  /usr/bin/install -c -m 644 units/user/systemd-exit.service '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/systemd/user'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/pkgconfig'
|  /usr/bin/install -c -m 644 shell-completion/zsh/_systemctl '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/zsh/site-functions'
|  /usr/bin/install -c -m 644 src/libsystemd/libsystemd.pc src/libudev/libudev.pc '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/pkgconfig'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/include/systemd'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-update-done /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-update-done
|  /usr/bin/install -c -m 644 src/core/systemd.pc src/udev/udev.pc '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/pkgconfig'
|  /usr/bin/install -c -m 644 ../git/src/systemd/sd-bus.h ../git/src/systemd/sd-bus-protocol.h ../git/src/systemd/sd-bus-vtable.h ../git/src/systemd/sd-event.h ../git/src/systemd/sd-login.h ../git/src/systemd/sd-id128.h ../git/src/systemd/sd-daemon.h ../git/src/systemd/sd-journal.h ../git/src/systemd/sd-messages.h ../git/src/systemd/_sd-common.h '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/include/systemd'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-update-utmp /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-update-utmp
|  /usr/bin/install -c -m 644 units/systemd-tmpfiles-setup.service units/systemd-tmpfiles-clean.service units/systemd-firstboot.service units/systemd-journald.service units/systemd-journal-flush.service units/systemd-journal-catalog-update.service units/systemd-coredump@.service units/systemd-vconsole-setup.service units/quotaon.service units/systemd-backlight@.service units/systemd-hostnamed.service units/systemd-networkd.service units/systemd-networkd-wait-online.service units/systemd-logind.service units/systemd-user-sessions.service '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/init.d'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-generators'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/var/log'
|  /bin/mkdir -p '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-modules-load /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-modules-load
|   ./arm-linux-gnueabi-libtool   --mode=install /usr/bin/install -c systemctl systemd-notify systemd-ask-password systemd-tty-ask-password-agent systemd-machine-id-setup systemd-escape systemd-tmpfiles systemd-firstboot udevadm systemd-hwdb journalctl networkctl loginctl systemd-inhibit '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin'
|  /usr/bin/install -c -m 644 docs/var-log/README '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/var/log'
|   ./arm-linux-gnueabi-libtool   --mode=install /usr/bin/install -c systemd-getty-generator systemd-fstab-generator systemd-system-update-generator systemd-debug-generator systemd-sysv-generator systemd-rc-local-generator systemd-gpt-auto-generator '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-generators'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-udevd /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-udevd
|  /usr/bin/install -c -m 644 docs/sysvinit/README '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/init.d'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c .libs/pam_systemd.so /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/security/pam_systemd.so
|   ./arm-linux-gnueabi-libtool   --mode=install /usr/bin/install -c systemd-cgls systemd-cgtop systemd-nspawn systemd-detect-virt systemd-delta systemd-analyze systemd-run systemd-stdio-bridge systemd-path busctl systemd-socket-activate systemd-cat coredumpctl hostnamectl '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c .libs/pam_systemd.lai /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/security/pam_systemd.la
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-journald /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-journald
| arm-linux-gnueabi-libtool: warning: remember to run 'arm-linux-gnueabi-libtool --finish /lib/security'
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-coredump /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-coredump
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-vconsole-setup /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-vconsole-setup
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-backlight /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-backlight
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-getty-generator /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-generators/systemd-getty-generator
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-hostnamed /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-hostnamed
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemctl /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/systemctl
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-fstab-generator /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-generators/systemd-fstab-generator
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-cgls /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/systemd-cgls
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-networkd /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-networkd
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-notify /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/systemd-notify
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-system-update-generator /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-generators/systemd-system-update-generator
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-cgtop /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/systemd-cgtop
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-networkd-wait-online /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-networkd-wait-online
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-debug-generator /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-generators/systemd-debug-generator
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-ask-password /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/systemd-ask-password
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-nspawn /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/systemd-nspawn
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-sysv-generator /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-generators/systemd-sysv-generator
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-logind /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-logind
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-detect-virt /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/systemd-detect-virt
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-tty-ask-password-agent /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/systemd-tty-ask-password-agent
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-rc-local-generator /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-generators/systemd-rc-local-generator
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-user-sessions /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/systemd-user-sessions
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-gpt-auto-generator /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-generators/systemd-gpt-auto-generator
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-machine-id-setup /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/systemd-machine-id-setup
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-delta /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/systemd-delta
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-escape /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/systemd-escape
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-analyze /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/systemd-analyze
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-tmpfiles /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/systemd-tmpfiles
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-run /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/systemd-run
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-firstboot /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/systemd-firstboot
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-stdio-bridge /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/systemd-stdio-bridge
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c udevadm /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/udevadm
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-hwdb /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/systemd-hwdb
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-path /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/systemd-path
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c journalctl /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/journalctl
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c busctl /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/busctl
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c networkctl /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/networkctl
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-socket-activate /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/systemd-socket-activate
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c loginctl /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/loginctl
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-cat /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/systemd-cat
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c systemd-inhibit /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/bin/systemd-inhibit
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c coredumpctl /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/coredumpctl
| make --no-print-directory install-data-hook
| arm-linux-gnueabi-libtool: install: /usr/bin/install -c hostnamectl /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/bin/hostnamectl
| make --no-print-directory install-exec-hook
| mv /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system/x-.slice /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image//lib/systemd/system/-.slice
| test -n "/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image" || /bin/systemd-hwdb update
| test -n "/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image" || /bin/journalctl --update-catalog
| what="" && wants=shutdown.target && dir=/lib/systemd/system &&        [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| /bin/mkdir -p /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/tmpfiles.d /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/tmpfiles.d /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/udev/rules.d /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/udev/hwdb.d /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/var/lib/systemd /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system/runlevel1.target.wants /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system/runlevel2.target.wants /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system/runlevel3.target.wants /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system/runlevel4.target.wants /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system/runlevel5.target.wants /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/modules-load.d /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/modules-load.d /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/systemd/network /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/systemd/network /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/sysctl.d /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/sysctl.d /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/kernel/install.d /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/kernel/install.d /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-shutdown /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-sleep /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/systemd/system-generators /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/systemd/user-generators /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/systemd/user /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/systemd/system /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/systemd/system/multi-user.target.wants /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/systemd/system/getty.target.wants /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/systemd/user /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/share/dbus-1/services /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/xdg/systemd
| set -- systemd-hostnamed.service dbus-org.freedesktop.hostname1.service      systemd-networkd.service dbus-org.freedesktop.network1.service systemd-logind.service dbus-org.freedesktop.login1.service poweroff.target runlevel0.target rescue.target runlevel1.target multi-user.target runlevel2.target multi-user.target runlevel3.target multi-user.target runlevel4.target graphical.target runlevel5.target reboot.target runlevel6.target graphical.target default.target reboot.target ctrl-alt-del.target getty@.service autovt@.service && \
|       dir=/lib/systemd/system &&      while [ -n "$1" ]; do /bin/mkdir -p `dirname /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$2` && rm -f /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$2 && ln -s $1 /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$2 && shift 2 || exit $?; done
| touch -c /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image//usr
| what="org.freedesktop.hostname1.busname org.freedesktop.systemd1.busname      org.freedesktop.network1.busname org.freedesktop.login1.busname" && wants=busnames.target && dir=/lib/systemd/system &&    [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| libname=libsystemd.so &&      if test "/usr/lib" != "/lib"; then /bin/mkdir -p /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib && so_img_name=$(readlink /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/$libname) && rm -f /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/$libname && lnr /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/$so_img_name /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/$libname && mv /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/$libname.* /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib; fi
| libname=libudev.so &&         if test "/usr/lib" != "/lib"; then /bin/mkdir -p /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib && so_img_name=$(readlink /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/$libname) && rm -f /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/$libname && lnr /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib/$so_img_name /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/$libname && mv /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/usr/lib/$libname.* /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/lib; fi
| /bin/mkdir -p /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/var/log/journal
| what="systemd-remount-fs.service tmp.mount var-lib-machines.mount" && wants=local-fs.target && dir=/lib/systemd/system &&     [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| chown 0:0 /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/var/log/journal
| chmod 755 /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/var/log/journal
| setfacl -nm g:adm:rx,d:g:adm:rx /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/var/log/journal/
| setfacl -nm g:wheel:rx,d:g:wheel:rx /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/var/log/journal/
| setfacl: Option -m: Invalid argument near character 3
| Makefile:22529: recipe for target 'journal-install-hook' failed
| make[4]: [journal-install-hook] Error 2 (ignored)
| what="systemd-logind.service systemd-user-sessions.service systemd-update-utmp-runlevel.service getty.target systemd-ask-password-wall.path" && wants=multi-user.target && dir=/lib/systemd/system &&    [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| what="" && wants=busnames.target && dir=/usr/lib/systemd/user &&      [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| what="systemd-update-utmp-runlevel.service" && wants=graphical.target && dir=/lib/systemd/system &&   [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| what="systemd-update-utmp-runlevel.service" && wants=rescue.target && dir=/lib/systemd/system &&      [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| what="ldconfig.service systemd-modules-load.service kmod-static-nodes.service systemd-tmpfiles-setup-dev.service systemd-tmpfiles-setup.service  systemd-firstboot.service systemd-machine-id-commit.service systemd-udevd.service systemd-udev-trigger.service systemd-hwdb-update.service systemd-journald.service systemd-journal-flush.service systemd-journal-catalog-update.service systemd-vconsole-setup.service   systemd-update-utmp.service systemd-update-done.service dev-hugepages.mount dev-mqueue.mount sys-kernel-config.mount sys-kernel-debug.mount sys-fs-fuse-connections.mount systemd-sysctl.service systemd-ask-password-console.path" && wants=sysinit.target && dir=/lib/systemd/system &&         [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| what="systemd-udevd-control.socket systemd-udevd-kernel.socket systemd-journald.socket systemd-journald-dev-log.socket systemd-journald-audit.socket systemd-coredump.socket systemd-initctl.socket" && wants=sockets.target && dir=/lib/systemd/system &&       [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| set -- /lib/systemd/system/shutdown.target shutdown.target /lib/systemd/system/sockets.target sockets.target /lib/systemd/system/timers.target timers.target /lib/systemd/system/paths.target paths.target /lib/systemd/system/bluetooth.target bluetooth.target /lib/systemd/system/printer.target printer.target /lib/systemd/system/sound.target sound.target /lib/systemd/system/smartcard.target smartcard.target /lib/systemd/system/busnames.target busnames.target && \
|       dir=/usr/lib/systemd/user &&    while [ -n "$1" ]; do /bin/mkdir -p `dirname /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$2` && rm -f /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$2 && lnr /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$1 /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$2 && shift 2 || exit $?; done
| what="systemd-tmpfiles-clean.timer" && wants=timers.target && dir=/lib/systemd/system &&      [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| what="" && wants=slices.target && dir=/lib/systemd/system &&  [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| what="" && wants=sockets.target && dir=/usr/lib/systemd/user &&       [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| what="" && wants=default.target && dir=/usr/lib/systemd/user &&       [ -z "$what" ] || ( dir=/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$wants.wants && /bin/mkdir -p -m 0755 $dir && cd $dir && rm -f $what && for i in $what; do ln -s ../$i . || exit $? ; done )
| set --   /lib/systemd/system/systemd-networkd.socket /etc/systemd/system/sockets.target.wants/systemd-networkd.socket /lib/systemd/system/systemd-networkd.service /etc/systemd/system/multi-user.target.wants/systemd-networkd.service /lib/systemd/system/systemd-networkd-wait-online.service /etc/systemd/system/network-online.target.wants/systemd-networkd-wait-online.service /lib/systemd/system/remote-fs.target /etc/systemd/system/multi-user.target.wants/remote-fs.target /lib/systemd/system/getty@.service /etc/systemd/system/getty.target.wants/getty@tty1.service /etc/systemd/user /etc/xdg/systemd/user /usr/share/dbus-1/system-services/org.freedesktop.systemd1.service /usr/share/dbus-1/services/org.freedesktop.systemd1.service && \
|       dir= &&         while [ -n "$1" ]; do /bin/mkdir -p `dirname /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$2` && rm -f /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$2 && lnr /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$1 /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image$dir/$2 && shift 2 || exit $?; done
| Making install in po
| make[2]: Nothing to be done for 'install'.
| ln: failed to create symbolic link '/home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/systemd/system/sysinit.target.wants/sync-clocks.service': No such file or directory
| WARNING: /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/temp/run.do_install.2299:1 exit 1 from 'ln -sf ../sync-clocks.service /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/image/etc/systemd/system/sysinit.target.wants/sync-clocks.service'
| ERROR: Function failed: do_install (log file is located at /home/nishihashi-na/tisdk-04.03.00.05/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/systemd/1_230+gitAUTOINC+3a74d4fc90-r0.arago5/temp/log.do_install.2299)
ERROR: Task (/home/nishihashi-na/tisdk-04.03.00.05/sources/oe-core/meta/recipes-core/systemd/systemd_230.bb:do_install) failed with exit code '1'