Part Number: AM3358
Hello,
I'm trying to build am335x processor sdk 6.01 using yocto bitbake.
Added meta-swupdate layer to source.
while using bitbake swupdate i'm getting following error.
========== /home/jigar/gcc-arm-8.3-2019.03-x86_64-arm-linux-gnueabihf/bin/../lib/gcc/arm-linux-gnueabihf/8.3.0/../../../../arm-linux-gnueabihf/bin/ld: cannot find -lubootenv collect2: error: ld returned 1 exit status Makefile:406: recipe for target 'swupdate_unstripped' failed make: *** [swupdate_unstripped] Error 1 ERROR: oe_runmake failed WARNING: /home/jigar/tisdk-am335x-build/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/swupdate/2019.11-r0/temp/run.do_compile.8721:1 exit 1 from 'exit 1' ERROR: Function failed: do_compile (log file is located at /home/jigar/tisdk-am335x-build/build/arago-tmp-external-arm-toolchain/work/armv7at2hf-neon-linux-gnueabi/swupdate/2019.11-r0/temp/log.do_compile.8721)
Added defconfig from custom layer.
# # Automatically generated file; DO NOT EDIT. # Swupdate Configuration # CONFIG_HAVE_DOT_CONFIG=y # # Swupdate Settings # # # General Configuration # CONFIG_CURL=y # CONFIG_CURL_SSL is not set # CONFIG_SYSTEMD is not set CONFIG_SCRIPTS=y CONFIG_HW_COMPATIBILITY=y CONFIG_HW_COMPATIBILITY_FILE="/etc/hwrevision" CONFIG_SW_VERSIONS_FILE="/etc/sw-versions" # # Socket Paths # CONFIG_SOCKET_CTRL_PATH="" CONFIG_SOCKET_PROGRESS_PATH="" CONFIG_SOCKET_REMOTE_HANDLER_DIRECTORY="/tmp/" # CONFIG_MTD is not set CONFIG_LUA=y CONFIG_LUAPKG="lua" # CONFIG_FEATURE_SYSLOG is not set # # Build Options # CONFIG_CROSS_COMPILE="" CONFIG_SYSROOT="" CONFIG_EXTRA_CFLAGS="" CONFIG_EXTRA_LDFLAGS="" CONFIG_EXTRA_LDLIBS="" # # Debugging Options # # CONFIG_DEBUG is not set # CONFIG_WERROR is not set # CONFIG_NOCLEANUP is not set # CONFIG_BOOTLOADER_EBG is not set CONFIG_UBOOT=y # CONFIG_BOOTLOADER_NONE is not set # CONFIG_BOOTLOADER_GRUB is not set CONFIG_UBOOT_FWENV="/etc/fw_env.config" # CONFIG_UBOOT_NEWAPI is not set # CONFIG_SSL_IMPL_NONE is not set CONFIG_SSL_IMPL_OPENSSL=y # CONFIG_SSL_IMPL_MBEDTLS is not set # CONFIG_DOWNLOAD is not set CONFIG_CHANNEL_CURL=y # CONFIG_HASH_VERIFY is not set # CONFIG_SIGNED_IMAGES is not set # CONFIG_ENCRYPTED_IMAGES is not set CONFIG_SURICATTA=y # # Features # CONFIG_SURICATTA_SSL=y CONFIG_SURICATTA_STATE_CHOICE_NONE=y # CONFIG_SURICATTA_STATE_CHOICE_BOOTLOADER is not set # # Server # CONFIG_SURICATTA_HAWKBIT=y # CONFIG_SURICATTA_GENERAL is not set CONFIG_WEBSERVER=y CONFIG_MONGOOSE=y CONFIG_MONGOOSEIPV6=y CONFIG_MONGOOSESSL=y CONFIG_GUNZIP=y # CONFIG_ZSTD is not set # # Parser Features # CONFIG_LIBCONFIG=y CONFIG_PARSERROOT="" CONFIG_JSON=y # CONFIG_LUAEXTERNAL is not set # CONFIG_SETSWDESCRIPTION is not set # # Image Handlers # CONFIG_RAW=y # CONFIG_RDIFFHANDLER is not set CONFIG_LUASCRIPTHANDLER=y CONFIG_SHELLSCRIPTHANDLER=y # CONFIG_HANDLER_IN_LUA is not set CONFIG_ARCHIVE=y CONFIG_REMOTE_HANDLER=y CONFIG_SWUFORWARDER_HANDLER=y # CONFIG_BOOTLOADERHANDLER is not set # CONFIG_UCFWHANDLER is not set
Thanks,