Other Parts Discussed in Thread: LM3S3634, SYSBIOS, LM3S3748
I'm trying to get our Stellaris project up and running with SYSBIOS on a dev board and for our design processor. We are using the EKS-LM3S3748 development board for now, but our eventual target processor is the LM3S3634. We're using CCS4.2. I need to get an RTSC platform file for these two processors. Is one available?
Also, when I try to create a new platform file from these, the first step is to choose the device family and device name. CortexM3 is available for selection as device family, but neither of my devices is then available in the drop down for device name. Is there a device file needed for these and is it available? If not available, which one would be a good starting point for creating a new one, and where do I find these files?
Thanks.