This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3503: can't get in contact with device

Part Number: OMAP3503


Hi guys,

Sorry had to put in OMAP3503 the real device is OMAP3621.

Our EMS has received OMAP 3621 with the marking 0800R1, which we have been unsuccessful to get to boot or get in contact with using JTAG.

Is it correct that this is a secure device and this behavior is expected?

Can we do anything to get it to boot and get in contact with it using JTAG?

Can you do anything so we can get it to boot and get in contact with it using JTAG?

Many thanks in advance

/Kim

  • Hi Kim,

     

    Based on the info you provided “OMAP 3621 with the marking 0800R1”, our internal check indicated that the device is High Secure (HS) device.

    The SW built for GP device can NOT boot on HS device as it is, and JTAG is disabled on HS by default.

     

    We’ll need to work with TI local sales team to get your purchased order corrected.

     

    Best,

    -Hong