This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354: GPMC RDACCESSTIME definition

Part Number: AM3354

Hi, 

My customer has a question about the define of of RDACCESSTIME of the register :GPMC_CONFIG5_0.

They are using the mode of GPMC:  Asynchronous Single Read Operation on an Address/Data Multiplexed Device.

In the Table 7-63 (P.725, http://www.ti.com/lit/ug/spruh73q/spruh73q.pdf), it says that ”Delay between start cycle time and first data valid”.

My customer want to know the define of "start cycle time". 

Does it means that when CSONTIME change from high to low is the  beginning of  "start cycle time"?

Thanks.