This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: FDTFILE override in Yocto

Part Number: PROCESSOR-SDK-AM335X

is there any easy way to override the default FINDFDT and/or FDTFILE variables built into the uboot source using a Yocto configuration script? 

it'd be really good not to have to manage a custom build of uboot just for a one-line hard-code change. Doesn't look like the later SDK supports uEnv.txt anymore, so I'm struggling to know where else to place a custom DTB file (other than overwriting an existing one with the same name)  

SDK version 06.02 - Kernel 4.19.78-rt