Part Number: AM4376
Other Parts Discussed in Thread: TMDSIDK437X
Hi Biser,
The DDR3 section of our board is based off of the schematic and layout of the AM437x Starter Kit and it works fine. In the SK pinout it seems all of the bits within the byte lanes are swapped including the prime "first" bit in each lane. However I just saw the posts "TMDSIDK437X: Single 16-bit DDR3" and "AM4376: AM4376BZDND80" where you say that the prime bit for each byte lane shouldn't be swapped. Is this a problem. What kind of issue could this cause? We are about to do a spin of the board, should we change the layout so that Bit0 of each byte lane isn't swapped? Or should we just leave it as is? I would rather not fix it if it isn't broke.
Thanks,
Bob