Part Number: AM3358
I have difficulties loading the "bone-debian-9.9-iot-armhf-2019-08-03-4gb.img" file to my custom controller board (or any boot file) via MMC0 SD card connection , based on AM3358 processor referring to Beaglebone Black. Despite it has same circuit configuration and boot setings as Beaglebone. I power up the circuit with SYSBOOT[4:0] 11000b pin settings as refer, but unlike reference design, nor indicator leds on my board blinks or image file copying starts. Evidence to AM3358 processor is alive are, exists "CCC..." terminal output responce on UART0 and there is 24MHz at CLKOUT1. I will be appreciate if any advice to solve the problem. Thanks,
Reyhan