This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ActiveSync and serial cable connection on 3530 EVM

Normal 0 false false false MicrosoftInternetExplorer4

Dear Sirs.

I newbie it this forum, sorry for very simple problem. :)

We are using OMAP 3530 TI BSP for Windows CE 6.0 for our engineering prototype.

I found that we can't create ActiveSync connection by serial port (we tried UART3 and UART1) since see no ActiveSync reaction. But for USB all is OK.

According to MSDN http://support.microsoft.com/kb/317171/en-us it should be done to init ActiveSync connection from device side. I didn't found any NOTIFICATION_EVENT_RS232_DETECTED generation in current BSP (TI_EVM_3530_6.15.00.zip).

Does TI OMAP BSP make signaling for Windows CE when serial link make available?

If yes then how to enable it?

If no then have got anybody solution and how to get it?

Thanks for help.