This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: WDT in U-boot

How to test watch dog timer in u-boot for beagle bone black?

  • Assuming by testing you mean seeing the watchdog timeout to confirm it is doing its job? For this you could just need to insert an endless loop at a suitable place in U-Boot, such as into the run_main_loop() function in common/board_r.c:

    static int run_main_loop(void)
    {
    #ifdef CONFIG_SANDBOX
    	sandbox_main_loop_init();
    #endif
    	/* main_loop() can return to retry autoboot, if so just run it again */
    	for (;;)
    		main_loop();
    	return 0;
    }

    In the above, if you comment out the invocation for main_loop(), you won't be periodically petting the watchdog, and the device should reset after a while.

    Regards, Andreas