This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA829V: Can LDC module of VPAC support rotation?

Part Number: DRA829V
Other Parts Discussed in Thread: DRA829

Hi, expert:

As customer's mechanical design, the camera module mount position is not as expected. The input video stream is about 130 degree angle. So it is needed to rotate the input camera video stream to 130 degree.

the camera module output format is YUV422.

My question is: Can LDC of VPAC support this kind of rotation (130 degree)?

(whether can it support 130 degree rotation of  YUV420 data)

Thanks.