Part Number: TDA4VM
Other Parts Discussed in Thread: SYSBIOS
After upgrading to PSDKRA 6.02 and PSDKLA 6.02, I am able to boot into the linux shell and run the vision app initialization script, but when I attempt to run a vision app I get the following IPC errors:
APP: Init ... !!!
APP_LOG: Mapping 0xac000000 ...
APP_LOG: Mapped 0xac000000 -> 0xffffb3640000 of size 262144 bytes
MEM: Init ION ... !!!
MEM: Initialized ION (fd=4) !!!
MEM: Init ION ... Done !!!
IPC: Init ... !!!
APP_LOG: Mapping 0xac040000 ...
APP_LOG: Mapped 0xac040000 -> 0xffffb16a0000 of size 33161216 bytes
APP_LOG: Mapping 0x30e00000 ...
APP_LOG: Mapped 0x30e00000 -> 0xffffb3b30000 of size 3072 bytes
rproc_device_find_for_name: could not open virtio node directory for r5f-main-0-core-1
IPC: ERROR: Unable to find rproc_device for rproc CPU [r5f-main-0-core-1]
IPC: ERROR: Unable to create TX channels for CPU [mcu2_1] !!!
IPC: ERROR: All local endpoints MUST be the same value, mismatch for CPU [mcu2_1] local endpt -1 != excpected local endpt 1024 !!!
IPC: Init ... Done !!!
APP: ERROR: IPC init failed !!!
REMOTE_SERVICE: Init ... !!!
rproc_device_find_for_name: could not open virtio node directory for r5f-main-0-core-1
IPC: ERROR: Unable to find rproc_device for rproc CPU [r5f-main-0-core-1]
rproc_device_find_chrdev_by_remote_port: could not find a matching rpmsg_chrdev node
IPC: ERROR: Unable to find rproc_char_device for rproc CPU [c66-0] @ remote endpt 21
rproc_device_find_chrdev_by_remote_port: could not find a matching rpmsg_chrdev node
IPC: ERROR: Unable to find rproc_char_device for rproc CPU [c66-1] @ remote endpt 21
rproc_device_find_chrdev_by_remote_port: could not find a matching rpmsg_chrdev node
IPC: ERROR: Unable to find rproc_char_device for rproc CPU [c7x] @ remote endpt 21
REMOTE_SERVICE: Init ... Done !!!
APP: Init ... Done !!!
I tried doing a fresh install of both the PSDKRA and PSDKLA in attempt to solve this error but I have not had any luck so far, any advice on how to resolve these errors would be appreciated.