Part Number: AM5718
I am intending to using the SPI3 lines in the AM5718 to program an external flash. There will also be another part on the same SPI lines that will use the data from the flash to execute it's program. Can all four of the AM5718 SPI lines (MOSI, MISO, CS, SCK) be tri-stated when they are not in use?