Hi,
The customer has a question about UART Baud Rate Setting described in Table 12-624 in AM65xx TRM. They want 115.2kbps, but its baud rate error becomes +0.16%.
Is it possible to minimize this error to 0% ?
If the external 48MHz oscillator (not internal PLL) was used as UART input clock, can it be 0% or lower ?
Regards,
Hideaki