Hi TI Support,
I tried building u-boot under.
ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/u-boot-2019.01+gitAUTOINC+66126341c8-g66126341c8
I built using below command
make u-boot_spl
The build was successful. In board-support/u-boot_build I can see two folders "a53" and "r5" . but I don't see the folder for a72 platform.
Below is the log from build process. I can see that it is building u-boot for A53 platform but using the config "j7313_evm_a72_config" Is this expected?
=================================== Building U-boot for A53 =================================== make -j 8 -C /home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/u-boot-* CROSS_COMPILE=/home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/aarch64-linux-gnu- \ j721e_evm_a72_config O=/home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/u-boot_build/a53 make[1]: Entering directory '/home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/u-boot-2019.01+gitAUTOINC+66126341c8-g66126341c8' make[2]: Entering directory '/home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/u-boot_build/a53' GEN ./Makefile # # configuration written to .config # make[2]: Leaving directory '/home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/u-boot_build/a53' make[1]: Leaving directory '/home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/u-boot-2019.01+gitAUTOINC+66126341c8-g66126341c8' make -j 8 -C /home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/u-boot-* CROSS_COMPILE=/home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/aarch64-linux-gnu- \ CONFIG_MKIMAGE_DTC_PATH=/home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/u-boot_build/a53/scripts/dtc/dtc \ ATF=/home/suddin/TI_ATF/bl31.bin TEE=/home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/prebuilt-images/bl32.bin \ O=/home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/u-boot_build/a53 make[1]: Entering directory '/home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/u-boot-2019.01+gitAUTOINC+66126341c8-g66126341c8' make[2]: Entering directory '/home/suddin/ti-processor-sdk-linux-automotive-j7-evm-06_01_01_02/board-support/u-boot_build/a53'
Best Regards
Sami