Part Number: 66AK2H06
Hi,
What does below code mean in arm rom code?
0x2501040 + (core number<<3)
0x1000030 + (core number<<2)
0x100_0030 is the address of AXI2BUSM Master.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: 66AK2H06
Hi,
What does below code mean in arm rom code?
0x2501040 + (core number<<3)
0x1000030 + (core number<<2)
0x100_0030 is the address of AXI2BUSM Master.
Nancy,
I am not sure that the code that you are referring to is ARM ROM code. ARM ROM code is not released either in binary or in source for 66AK2H06 device so please let us know which source file you are seeing the reference code. If ROM code was shared with you privately in the past then we need to take the discussion offline to support this effort.
Regards,
Rahul