I have a question as to whether the C6727 specifically supports AET, and whether the AET can be made to trigger an interrupt as opposed to having to have the emulator connected. In some DSPs I have found some talk in the forums that it can using "AETLib". I have found a Tech Note that says that in principle the C6713 can do this, but that it depends for each DSP what mega-module it is. If the megamodule is "Full-GEM", then apparently it can.
So does anybody know whether the C6727 is full-GEM? And if it is, does AETLib support C6727? AETLib is part of "CTools"
In case people are wondering what I am trying to do, I would like to set Advanced Event Triggering up to identify stack overflow in the field, immediately in 4 clock-cycles.