From the data sheet:
6.11.3.12 MDDR/DDR2 Boundary Scan Limitations
Due to DDR implementation and timing restrictions, it was not possible to place boundary scan cells
between core logic and the IO like boundary scan cells for other IO. Instead, the boundary scan cells are
tapped-off to the DDR PHY and there is the equivalent of a multiplexer inside the DDR PHY which selects
between functional and boundary scan paths.
The implication for boundary scan is that the DDR pins will not support the SAMPLE function of the output
enable cells on the DDR pins and this is a violation of IEEE 1149.1. Full EXTEST and PRELOAD
capability is still available.
I’m not fully up to speed on boundary scan testing, what impact does this have on real world testability?