Part Number: TDA4VM
Tool/software: TI C/C++ Compiler
Hi TI members:
Because our project target is set DPI1 to output YUV422 format and have 12 data pins to Serializer MAX96715,
In this premise, I find this document http://www.ti.com/lit/an/spracg3/spracg3.pdf form other ticket,
But I still have a few questions:
1. Is spracg3.pdf way still available on TDA4 platform?
2. How to set DPI1 as "2.1 Emded Sync Output" ,
Because there are two output way "Emded Sync output" & "Discrete Sync output",
Is DSS0_VP_CONFIG register 24bit & 20 bit enough to achieve our goal ??
3. Is there related patch on TDA4 platfom about set panel-timing to BT601 uyvy 30fps & TDM Mode ?
like the patch download form spracg3.pdf's link "www.ti.com/.../spracg3"