Part Number: TDA4VMXEVM
Hi,
after some searching I've been able to find a tutorial on the E2E forums which shows how to import Tensorflow models into TIDL:
The tutorial seems to be out of date, as I had to adjust many file names and many paths. In the end I've been able to convert mobilenet v1 into TIDL format.
However, when I run the inference simulation, I get the following error:
Processing config file #0 : testvecs/config/infer/public/tensorflow/tidl_infer_mobileNetv1.txt
----------------------- TIDL Process with REF_ONLY FLOW ------------------------
# 0 . .. T 948.16 ... A : 896, 0.0000, 0.0000, 670 .... .....
# 1 . .. T 908.94 ... A : 558, 0.0000, 0.0000, 420 .... .....
# 2 . .. T 901.69 ... A : 443, 0.0000, 0.0000, 420 .... .....
# 3 . .. T 897.74 ... A : 499, 0.0000, 0.0000, 420 .... .....
# 4 . .. T 909.30 ... A : 539, 0.0000, 0.0000, 420 .... .....
# 5 . .. T 896.48 ... A : 539, 0.0000, 0.0000, 420 .... .....
# 6Error in reading �̽��, �̽��
----------------------- TIDL Process with REF_ONLY FLOW ------------------------
# 0 . .. T 948.16 ... A : 896, 0.0000, 0.0000, 670 .... .....
# 1 . .. T 908.94 ... A : 558, 0.0000, 0.0000, 420 .... .....
# 2 . .. T 901.69 ... A : 443, 0.0000, 0.0000, 420 .... .....
# 3 . .. T 897.74 ... A : 499, 0.0000, 0.0000, 420 .... .....
# 4 . .. T 909.30 ... A : 539, 0.0000, 0.0000, 420 .... .....
# 5 . .. T 896.48 ... A : 539, 0.0000, 0.0000, 420 .... .....
# 6Error in reading �̽��, �̽��
Can you help us get in touch with some TI expert who may help us understand the problem ?
Also, the neural networks we need to test are the following:
SSD-RESNET34
RESNET-50 V1.5
MOBILENET-V1 224
I haven't found any tutorial (or freeze scripts) for ssd-resnet34 and resnet-50 1.5. We need your support in trying to port these, too.
Kind regards,
one and zero