Hi,
I am working on custom board TDA2px. I am trying to add tidl_OD usecase.
Usecase built successfully but I am getting runtime error as follows
[IPU1-0] 11.802934 s: dispcore/src/vpscore_dss.c @ Line 1404:
[IPU1-0] 11.803025 s: Input width+posx/height+posy > display width /height
[IPU1-0] 11.803147 s: dispdrv/src/vpsdrv_displayCore.c @ Line 304:
[IPU1-0] 11.803208 s: Set DSS parameter failed
[IPU1-0] 11.803269 s: Assertion @ Line: 466 in displayLink_drv.c: status==SYSTEM_LINK_STATUS_SOK : failed !!!
[IPU1-0] 11.803757 s: Assertion @ Line: 466 in displayLink_drv.c: status==SYSTEM_LINK_STATUS_SOK : failed !!!
Input video size is 768 X 360. I have not changed any display parameters from original tidl_OD usecase