This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6745: GPIO Low level driver

Part Number: TMS320C6745

First of all i'm a newbie.

Referencing the GPIO LLD in pdk_omapl137_1_0_10, it seems to me that there is a problem on the GPIO_v0_hwAttrs 

It is in  defined GPIO_soc.c as

/* GPIO Driver hardware attributes */
GPIO_v0_hwAttrsList GPIO_v0_hwAttrs =
{
{
CSL_GPIO_0_REGS,
&GPIO_intCfgs[0][0],
NULL
}
};

It is used in GPIO_V0.c as

GPIO_v0_hwAttrs[portNum];

In this way only port 0 is working (only 1 item in the array), and port 0 is the port used in the led blink demo.

But i need a GPIO in other ports, and would prefer do not change the pdk