Dear all,
My sw is dvsdk4.00, hw is dm365.
When SingleShot-Resize set a high clock divider, eg., 1/2, 1/3, the driver may die at the function "wait_for_completion_interruptible(&(imp_serializer_info.sem_isr)" because of the irq of resize is missed and can't resume from this error condition.
I thought this is caused by the ddr2 bandwidth starvation. If I don't want to reduce my resize clock, can I get a error interrupt and some status register-bit to stand dor this error condition?
Please help me. Thank you!
Wei Jiang