Part Number: SYSBIOS
Other Parts Discussed in Thread: AM3352
CCS 9.3.0
SYSBIOS 6.76.02.02
XDC tools 3.55.02.22
ti-processor-sdk-rtos-am335x-evm-06.01.00.08-Windows-x86-Install
OS: Windows 10 1909, 64 bit.
Target is a custom AM3352 board which currently runs my full application built on earlier versions of CCS/SYSBIOS/XDC Tools.
After installing CCS and the SDK, I imported a sysbios Hello World project from the SDK and attempted to build it.
I get an error in the XDC tools build:
js: "./config.bld", line 10: Error: Can't find the target named 'ti.targets.arm.elf.A8Fnv'
The A8Fnv target files are not in the SYSBIOS package path where it is looking..
I went back to the development PC for my production application, and found that target where I expected it to be in the SYSBIOS 6.45.1.29
Is there something I have to do to get the A8Fnv target to show up in the newer SYSBIOS?
Gerry Belanger