Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI C/C++ Compiler
Hi all,
I am facing the following error in building TI ndk package.
C:\ndknsp_packages\ndk_2_24_02_31>C:\ti\xdctools_3_30_03_47_core\gmake.exe -f ndk.mak clean
cleaning ndk packages ...
C:\ti\xdctools_3_32_01_22_core\bin\stderr.exe: can't execute 'echo "making" "clean:" "because:" "Invalid" "argument" "C:\ti\xdctools_3_32_01_22_core\bin\stderr.exe:" "can't" "execute" "'date" "'" "(exit" "status" "=" "-1)" "..." ' (exit status = -1) because: Invalid argument
xdctools_3_32_01_22_core\gmake.exe: *** [_startime] Error 255
gmake: *** [clean] Error 2
Following the following html path for build steps:
C:\ndknsp_packages\ndk_2_24_02_31\ndk_2_24_02_31_release_notes.html
Please find the ndk.mak below:
------------------------------------------------------------------------------------------------------------
#
# ======== ndk.mak ========
#
#
# Where to install/stage the packages
# Typically this would point to the devkit location
#
DESTDIR ?=
prefix ?= /
docdir ?= /docs/ndk
packagesdir ?= /packages
# USER STEP: user must define below path to xdc installation
# Set up dependencies
XDC_INSTALL_DIR ?= C:/ti/xdctools_3_32_01_22_core
SYSBIOS_INSTALL_DIR ?= C:/ti/bios_6_46_04_53
#
# Set location of various cgtools
# These variables can be set here or on the command line.
#
# USER STEP: user must define below paths to compilers
ti.targets.C64P ?=
ti.targets.C64P_big_endian ?=
ti.targets.C674 ?=
ti.targets.elf.C66 ?= C:/ti/c6000_7.4.2
ti.targets.elf.C66_big_endian ?=
ti.targets.elf.C674 ?=
ti.targets.arm.elf.Arm9 ?=
ti.targets.arm.elf.A8F ?=
ti.targets.arm.elf.A8Fnv ?=
ti.targets.arm.elf.M3 ?=
ti.targets.arm.elf.M4 ?=
ti.targets.arm.elf.M4F ?= C:/ti/arm_5.2.4
gnu.targets.arm.M3 ?=
gnu.targets.arm.M4 ?=
gnu.targets.arm.M4F ?=
gnu.targets.arm.A8F ?=
gnu.targets.arm.A9F ?=
gnu.targets.arm.A15F ?= C:/ti/gcc-arm-none-eabi-4_7-2013q3
iar.targets.arm.M3 ?=
iar.targets.arm.M4F ?=
iar.targets.arm.M4 ?=
# Set BUILDMINSTACK to 1 to only build base stack libraries (stk.a* and stk6.a*)
BUILDMINSTACK ?= 0
#
# Set XDCARGS to some of the variables above. XDCARGS are passed
# to the XDC build engine... which will load ndk.bld... which will
# extract these variables and use them to determine what to build and which
# toolchains to use.
#
# Note that not all of these variables need to be set to something valid.
# Unfortunately, since these vars are unconditionally assigned, your build line
# will be longer and more noisy than necessary (e.g., it will include CC_V5T
# assignment even if you're just building for C64P).
#
# Some background is here:
# rtsc.eclipse.org/.../Command_-_xdc
#
XDCARGS= \
ti.targets.C64P=\"$(ti.targets.C64P)\" \
ti.targets.C64P_big_endian=\"$(ti.targets.C64P_big_endian)\" \
ti.targets.C674=\"$(ti.targets.C674)\" \
ti.targets.arm.elf.Arm9=\"$(ti.targets.arm.elf.Arm9)\" \
ti.targets.arm.elf.A8F=\"$(ti.targets.arm.elf.A8F)\" \
ti.targets.arm.elf.A8Fnv=\"$(ti.targets.arm.elf.A8Fnv)\" \
ti.targets.arm.elf.M3=\"$(ti.targets.arm.elf.M3)\" \
ti.targets.arm.elf.M4=\"$(ti.targets.arm.elf.M4)\" \
ti.targets.arm.elf.M4F=\"$(ti.targets.arm.elf.M4F)\" \
ti.targets.elf.C66=\"$(ti.targets.elf.C66)\" \
ti.targets.elf.C66_big_endian=\"$(ti.targets.elf.C66_big_endian)\" \
ti.targets.elf.C674=\"$(ti.targets.elf.C674)\" \
gnu.targets.arm.M3=\"$(gnu.targets.arm.M3)\" \
gnu.targets.arm.M4=\"$(gnu.targets.arm.M4)\" \
gnu.targets.arm.M4F=\"$(gnu.targets.arm.M4F)\" \
gnu.targets.arm.A8F=\"$(gnu.targets.arm.A8F)\" \
gnu.targets.arm.A9F=\"$(gnu.targets.arm.A9F)\" \
gnu.targets.arm.A15F=\"$(gnu.targets.arm.A15F)\" \
iar.targets.arm.M3=\"$(iar.targets.arm.M3)\" \
iar.targets.arm.M4F=\"$(iar.targets.arm.M4F)\" \
iar.targets.arm.M4=\"$(iar.targets.arm.M4)\" \
BUILDMINSTACK=\"$(BUILDMINSTACK)\"
#
# Set XDCPATH to contain necessary repositories.
#
XDCPATH = $(SYSBIOS_INSTALL_DIR)/packages
export XDCPATH
#
# Set XDCOPTIONS. Use -v for a verbose build.
#
#XDCOPTIONS=v
export XDCOPTIONS
#
# Set XDC executable command
# Note that XDCBUILDCFG points to the ndk.bld file which uses
# the arguments specified by XDCARGS
#
XDC = $(XDC_INSTALL_DIR)/xdc XDCARGS="$(XDCARGS)" XDCBUILDCFG=./ndk.bld
######################################################
## Shouldnt have to modify anything below this line ##
######################################################
all:
@ echo building ndk packages ...
@ $(XDC) -Pr ./packages
clean:
@ echo cleaning ndk packages ...
@ $(XDC) clean -Pr ./packages
install-packages:
@ echo installing ndk packages to $(DESTDIR) ...
@ mkdir -p $(DESTDIR)/$(prefix)/$(docdir)
@ cp -rf $(wildcard ndk_*_ReleaseNotes.html) docs/* $(DESTDIR)/$(prefix)/$(docdir)
@ mkdir -p $(DESTDIR)/$(prefix)/$(packagesdir)
@ cp -rf packages/* $(DESTDIR)/$(prefix)/$(packagesdir)
----------------------------------------------------------------------------------------------------------------
Doubly verified all the paths of ti packages and ti compilers but still i am facing the build error.
Please help in resolving the above mentioned error:
Regards
Mayank