This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP-L138 SATA Interface Clock Source - LVPECL instead of LVDS

Expert 1070 points


Hi all,

The OMAP-L138 DS states that  "the SATA interface requires a LVDS differential clock source to be provided at signals SATA_REFCLKP and SATA_REFCLKN".

The last DS revision (sprs586b) specifies only the minimum value (250 mV) of  the Differential Clock Input voltage.

What is the maximum allowable value?

And can the LVPECL clock source be used taking into account the capacitive coupling recommended for that clock input?