Part Number: TMDSDSK6713
Is it possible to use and program DSP kit c6713 through python? If yes ,how?Please kindly guide,through which version of python and how?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSDSK6713
Is it possible to use and program DSP kit c6713 through python? If yes ,how?Please kindly guide,through which version of python and how?
This is not the general way we recommend customers to program our DSPs. This is a DSP only device, which comes with a TI provided C/C++ compiler which you can use for development. The CCS IDE also has interface to build projects using the above mentioned compiler. Generally only TI platforms on which you can program or run python code are device which have ARM integration with high level OS like Linux running on it.
Regards,
Rahul