Part Number: TDA4VMXEVM
I'm trying to reproduce the lspci output described in section 3.2.2.10 of the "Processor SDK Linux Automotive" documentation. I've plugged in a PCIe x1 Ethernet adapter and then powered on to boot the prebuilt SD card image (version 06_02_00). DIP switches SW3.5 and SW3.6 are set to '1' to operate the board in Root Complex mode. Although the RC should enumerate any off-the-shelf PCIe cards, lspci only shows the PCI bridges:
root@j7-evm:~# lspci 0000:00:00.0 PCI bridge: Texas Instruments Device b00d 0001:00:00.0 PCI bridge: Texas Instruments Device b00d 0002:00:00.0 PCI bridge: Texas Instruments Device b00d
I've verified that the Ethernet adapter runs fine in a normal PC. As this test is very basic I suspect an issue with my evaluation board instance. Could you please verify that the prebuilt Linux image correctly enumerates the bus without any further configuration as described in the documentation?
Regards,
Tom