This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[DRA829] Compiler uniflash project in SDK 2.0 package

Other Parts Discussed in Thread: UNIFLASH

HI,expert

I compiler the uniflash project in the SDK2.0 package, and I set the MCU to UART mode , then download the uart_j721e_evm_flash_programmer_release.tiimage thouge UART, it doesn't work!!!!! 

Is that same with you??

Hope to reply as soon as possible!

Regards,

Xie

  • Hi Xie,

    Can you please explain the problem a little more - I would like to understand what you mean by it doesn't work?

    Some logs or more description will help in getting you some help on this.

    Also, it would be good if you can provide the Uniflash version and the SDK version too - what is SDK 2.0 package? Please share complete name of the SDK.

    Regards

    Karthik