This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCI6638K2K: TCI6638K2K

Part Number: TCI6638K2K


Hi,

High undershoot/overshoot coming on 100 MHz diff clock  on  PCI-Reference clock input connected to DSP. External AC coupled LVDS  clock is given to this input.

 

Q1.  H/W design  says the input clock buffer for PCIECLKn/p are having internal termination of 100 ohm? Is there any setting to be done to enable this 100 ohm Res or it’ll be enabled by default?

 

Q2. Is the input buffer for PCIECLJn/p a CML buffer, In Datasheet it’s mentioned serdes/cml, pl. refer page 34 of HW design guide.  What is serdes buffer? What will be the default setting for it, CML or serdes buffer?

 

Q3. HW design guide also says these serdes reference clocks are internally AC coupled. Pl. refer page 35. So do we need to put external AC cap, or LVDS clock at 3.3V can be directly connected.

 

 

One observation: if we put external Res of 100 ohm then the clocks are becoming fine. CML input buffers  have the internal termination Res and biasing ckt. I doubt the PCICLKn/p to come-up in CML mode needs some settings to be done..?