We are using a 5505A with the CSL and USB. The USB fails to connect to a PC at power on. If we reset the hardware the USB connects to the PC. The problem only occurs on Power on. We are using the CSL that was released this summer and we have the 5505 define set correctly.
We have tried to use the XDS510 debugger to look at the problem, but whenever we use the debugger, the USB connects.
Any ideas.