WARNING: On a Linux development host, Never ever ever ever Never ever Never Never try to use one of the makefiles in DVSDK 3.10 (and probably others) aside from the primary makefile in the higher level folder next to Rules.make.
The individual makefiles are just too convoluted and too sensitive to work without loads of trouble and wasted time. This is even in SPITE of the instructions that come with things like DSP Link, which suggest using lower level makefiles. For DSP Link, don't follow the instructions. Just run "make dsplink" or "sudo make dsplink" at the top level.
And when it comes to a Windows XP development host, I'm not sure if that high level make works, either. There seem to be many slash problems (forwardslash versus backslash), as well as differences in opinion as to where files MUST be installed for CCS vs DVSDK. I had to brute force the makefiles under CCSv4 and finally get things working just to compile a codec and server. I don't have the time to try again going from the DVSDK top level makefile.
NEVERTHELESS, note that this top level makefile in DVSDK comes with its own problems. Mine still won't run all the way through without error when I simply try "make". This is one reason, combined with the instructions for DSP Link found in the UserGuide.pdf, that I didn't get things done in the beginning by the top level make. I had to separately do the "sudo make dsplink" (sudo for me) and "make demos" to get things working. Note my objective in all this was to do little more than tweak the ividanalytics_copy codec and the encodedecode demo, then rebuild them to try out on the EVM.
-Helmut
P.S. Sincere sincere thanks to many folks who helped me along the way. I know a lot more about the "surface streets" (that I really had neither time nor therefore need to learn, unfortunately). But now I just ran on the express freeway to get very close to where I need to be on this project.
ADVICE TO TEXAS INSTRUMENTS: On the next DVSDK release, add a special internal env var that the top level makefile sets to point out the fact that it's running. Then in EVERY makefile anywhere in the DVSDK, check for that env var. If not present/set, output an obvious warning (like surrounded by * or = chars) that things will be much, much easier if you run the top level makefile. Even give advice as to the parameter to pass, such as "make demos" advice coming from encodedecode/Makefile.