Other Parts Discussed in Thread: OMAPL138
Hi,
In terms of the DDR2 interface to the OMAP L138 processor, would the OMAP-L138 be able to support a dual-memory DDR2 configuration with each memory of 256Mx8bit in size? In this case, as it has two DDR2 SDRAM devices, the total DDR2 memory size will be 256Mx8bit x 2, ie 512MB or 4Gb. Is this equivalent to a single-memory configuration with 256Mx16bit in size? If so, would the software be the same to run the two configurations? In other words, is the software going to see any differences to the two configurations?
Thank you very much for your help in advance!
Best regards,
Wenbo