Other Parts Discussed in Thread: TPS65910
Hi,
My customer make a design for AM3354BZCZ80 and it can boot successfully.
Then they change the main chip from AM3354BZCZ80 to AM3354BZCZ100.
But the PCBA w/AM3354BZCZ100 boot fail at U-BOOT.
The following is the info from my customer:
1. VDD core from TPS65910 : 1.325 V
2.U-BOOT fail log:
U-Boot SPL 2013.01.01-bbb-fb (Nov 02 2019 - 19:52:51)
am33xx_spl_board_init
mpu_pll=1000
pmic=TPS65910
OMAP SD/MMC: 0
reading u-boot.img
spl: error reading image u-boot.img, err - -1
### ERROR ### Please RESET the board ###
3. The layout of CPU and DDR3 is referenced from beagle bone, but the PCBA is 10 layers.
Please help to provide comments for booting successfully.
Thanks.