This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EXEVM: channel switching in single channel display.

Part Number: TDA2EXEVM

Hello there,

We are having an use-case  for 6-channel display.

Capture(6-channels) -> VPE -> Merge -> Display.

For switching between the channels  we are using the below API,

Int32 System_linkControl(UInt32 linkId, UInt32 cmd, Void *pPrm, UInt32 prmSize, Bool waitAck)


If we want to switch the API, the parameter "params.activeChId"  from structure

typedef struct
{  
    UInt32                   activeChId;
    /**< Active chID from which frames should be displayed */
} DisplayLink_SwitchChannelParams;

are assigned the value to change the channels.

But every-time channel 0 is displayed first. even though we have changed the  activeChId to some other value not 0.

For our requirement we need to display data based on the activeChId value.

Please suggest the solution.

Thanks & regards

Balaji T