I have a sensor in YUYV format. In the CCDCCFG register, bit 11 (YPOS) is supposed
to set the position of Y to odd or even pixel.
On my dm365, this bit has no effect.
Here is my dataflow :
sensor -> ccdc -> ddr
ddr -> ipipe (resizer) ->ddr->display
With an UYVY sensor, Y and U/V are not swapped
With an YUYV sensor, Y and U/V are swapped, wether the Y8POS bit is set or not
I have seen a post with a similar problem on DM368, where it is said the Y8POS bit
works only when moving data to DDR. However, I am in this case, and I can see no difference.