Part Number: AM5718
Hello
I am using am5718 custom board.
I want to communicate rs485 using am5718 uart4.
The RS-485 control pin (RE, DE) pin uses GPIO.
But there is a problem.
RS-485 control pins (RE, DE) are not connected to uart4_rts, uart4_cts, so txd and rxd lines cannot be controlled. If you try to write after controlling a simple gpio, there is a problem because the time when the write is completed is not known.
Is there any way to use rs-485 without rts, cts pin?