Other Parts Discussed in Thread: OMAPL138
Hello,
I have few doubts for using OMAP L138 in my custom made board.
Firstly i want to know what boot mode settings i need to do for programming my SPI flash thru' UART. Pl note i am using 25MHz input clock. So whether i need to change the boot mode pins 7-5 to 110, if yes then whether i can use the same ubl code which is used for EVAL baord ?
Second is if i program my SPI flash via JTAG then after booting from SPI Flash whether i will need to set the boot mode pins 7-5 to 110 for a 25MHz input clock to successfully communicating via UART ? Will the same ubl code (used for Eval board) be able to boot the processor or not that's also doubtfful.
Thanks
Ajay