This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SDHC MMC is not getting detected on my customized DM365 board



Hi,

On my customized DM365 board, I have two MMC ports. Following are details of components I am using,

DVSDK: dvsdk_2_10_01_18

Toolchain: MVL 5.0

Kernel: 2.6.18

PSP: 2.10.00.14

I applied the patch available at http://processors.wiki.ti.com/index.php/How_to_use_SDHC_on_DM365_with_MontaVista_5.0

After applying this patch,  I am able to detect and mount 4GB Sandisk MMC on port 0 but the same card is not getting detected on the port 1.

Can anyone tell me what could be the problem? Do I need to make any board specific change after applying this patch?

--

Alok Bhatt