Other Parts Discussed in Thread: ADS1158
Hi
I'm using the C6742 in a design with the ADS1158 connected via SPI. (Well, that's the plan. For now the ADS1158 is connected to SPI from the C6748 EVM until HW design is finished.) I use DSP/BIOS 5.41.
I guess I'll have to write an SPI driver for the ADS1158, but I'm a bit at loss how the standard SPI driver in DSP/BIOS works. I've read the "DSP/BIOS SPI Device Driver Architecture/Design Document" (from pspdrivers_01_30_00_05\packages\ti\pspiom\spi\docs), but it is still not very clear to me.
Are there any other documents on SPI in BIOS or the C674x? Or is there some example code?
Also: if there is some sample code to interface the ADS1158 with DSP/BIOS, I'd be a very happy man.
Best regards
Admar